Part Number: P82B96
Hi,
Could you kindly advise the specification of VOL for Tx, Ty like Sx, Sy ?
Thank you and best regards,
Michiaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: P82B96
Hi,
Could you kindly advise the specification of VOL for Tx, Ty like Sx, Sy ?
Thank you and best regards,
Michiaki
Hi Michiaki,
We don't specify these values because it can vary widely based on the conditions of the device. Since Rx,Ry have a wide input threshold (0.5xVcc typ) and the Tx,Ty driver strength is so large, we don't typically see an issue here.
As an example estimate, we can divide the test conditions of Vtx = 1V by the Dynamic output sink capabilities (Iiot) of Tx,Ty of 60mA MIN to get an Rds(on) of ~16.7-Ohm. Using a Rpu value of 160-Ohm, the Vol would come out to be near 9%Vcc. Note that this value will vary with the amount of sink current, Rpu values, and temperature.
Regards,
Eric