Part Number: DS125DF410
Other Parts Discussed in Thread: DS110DF410
Hi TI team,
This is in continuation of our old discussion in earlier thread done during design stage.
As per this we concluded that we will be using the part no: DS125DF410 @ Data Rate : 1.0625Gbps
Data Path: Transceiver Tx ---> Retimer --> AC Coupling Caps (0.22uF) --> Transceiver Rx
We have received the fabricated boards and are in testing phase. Below are our observations:
1. No data received at the Transceiver Rx. We have probed the data at the input of the retimer, we see the data lines toggling and the eye is visible. But at the output of the retimer data is not present - Lines are not toggling and is stable at 1.3V, No Data, No eye.
2. We replaced AC Coupling Caps with 0 ohm and shorted the path, no difference in the retimer output as well as the Transceiver - Rx
3. We bypass the retimer and tested.
Transceiver - Rx is able to capture & lock to the incoming data and all the test patterns are passing.
After re-reviewing from other team we have below doubts :
Data Rate supported by the Retimer is from 9.8 Gbps to 12.5Gbps, but since the data rate at which we are operating is 1.0625Gbps, will the VCO and the CDR locks to the data, if so what all configuration has to be done in the Retimer.
Consider this as the high priority as we have received the fabricated boards & it has become a bottleneck for our testing.
Thanks & Regards,
Ananthesh