Part Number: HD3SS3415
Hello,
According to Revision History section, temperature changed from: industrial temperature range of –40°C to 85°C to: industrial temperature range of 0°C to 70°C.
Is this change only related to performances, or is this a maximum operating rating ?
For example, is there any problem with supplying power to the component at -10 °C (no performance required) ?
Best regards,
Christian