This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Question for CSI-2 setting

Part Number: DS90UB954-Q1


Hi Team,

My customer asked CSI-2 setting for below specific case.

Could you check if below settings are reasonable to have sufficient bandwidth?

<<  System requirement >>

1. configuration : CMOS sensor + 953 + 954 (single 953 is connected)

2. streaming data : 1920x1080x60fps, 12bit/pixel (Raw12bit)

     --> 1.64Gbps with Blanking rate =1.1

3. max 1.5Gbps for ISP lane

<< DS90UB954 configuration >>

1. For FPDLINK setup for non-synchronous CSI-2 mode

set FPD3_MODE = "00",

REFCLK = 25MHz(from xtal oscillator)

2. For CSI-2 setup

From Table 13, to set CSI frequency less than 1.5Gbps with REFCLK=25MHz,

(1) CSI_PLL_CTL[1:0] has to be set as "00"

(2) IND_ACC_CTL[5:2] =  "0111"

(3) IND_ACC_ADDR = 0x08

(4) IND_ACC_DATA[7:6] = "11" (csi pll divider setting = 52)

(5) CSI_LANE_COUNT = "10" (2 lane)

With this setting, I expect 954 has 1.3Gbps x 2 lane capability.

Best regards,

Nobuo