Part Number: TCA9800
Other Parts Discussed in Thread: TCA9803
Dear Team,
Currently, the customer use TCA9800 connect between PU6 and PU4.
TCA9800 A side connect to PU6, B side connect to PU4.
With 3.3V and 1.5kohm pull high.
Since the PU4 input need under 0.4V.
Is there any method can have lower low level voltage here?
Is TCA9803 will help here?
BR
Kevin