Part Number: LMH0376
Other Parts Discussed in Thread: LMH0346, LMH0366, , LMH1226, LMH0318, LMH0397, LMH1219EVM
Hello TI support,
I'm looking for a 3G-SDI reclocker (to reclock 3G-SDI inputs coming into our board) that have, the following features:
- Ideally a single 2.5V power supply
- Ideally no external clock need
- Mandatory : Operational through pin strapping only (no SPI/SMbus)
I identified the following parts:
- LMH0346 but it requires 3.3V and an external clock
- LMH0366 but according to the threat below, it can be needed to program it first through SPI to have good performance
https://e2e.ti.com/support/interface/f/138/t/464320?tisearch=e2e-sitesearch&keymatch=LMH0366
- LMH0376 seems to meet all my needs
So actually, I think the LMH0376 is the most suited device considering my needs.
Can you please confirm?
Or do have other parts to suggest ?
Thank you,
Yann