Part Number: DP83849IF
Hi,
I have gone through the below post/thread for testing BIST in external loopback.
https://e2e.ti.com/support/interface/f/138/p/225948/805414
I did BIST in external loopback using loopback cable by following below steps in firmware:
1. Set the LOOPBACK bit of BMCR register to 1
2. Set the BIST_START bit of PHYCR registe to 1
3 Then read the BIST_STATUS bit of PHYCR, to check whether it is a 1(pass) or 0(fail)
The BIST_STATUS bit of PHYCR shows 1-pass.
Are all the above steps to test BIST in an external loopback correct? , or do I need to enable PMD_LOOPBACK bit in RBR register?
Many Thanks.
Yash