If the TCA9554A is not powered on VCC, but inputs (specifically SCL and SDA) are pulled up to a 3.3 volt standby supply via a pull-up resistor, what amount of current leakage will occur to VCC?
The datasheet indicated that if SCL or SDA is at a higher potential than VCC, the leakage current (IsubL) will increase above the +/- 1 mA level, but is it not clear what the leakage amount will be and if the path is to Vcc, to GND, or to both.