Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65983B
Hello,
My customer wants to use 2 pcs of TPS65987D to replace the TPS65983B in reference design TIDA-03027 with the updated block diagram as following:
Q1: TPS65983B use UART interface to share firmware between 2 devices. Does it work using I2C between 2 TPS65987D?
Q2.Tpye A port is not needed. So customer can eliminate USB billboard, right?
Q3,Q4, One HDMI 2.0 port is needed and the typc-C port will also be used to transmit video signal. What is the correct configuration of the SS MUX and TX/RX pairs?
Best regards,
Victor