Part Number: SN65LVDT3486B
I can't find thermal resistances on SN65LVDT348PWRG4. It is the TSSOP package. I would like to know
theta jc
theta jb
theta ja
pin material
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65LVDT3486B
I can't find thermal resistances on SN65LVDT348PWRG4. It is the TSSOP package. I would like to know
theta jc
theta jb
theta ja
pin material
I will request thermal data, but may take couple of days.
Here are the thermal parameters
| Theta JA-High K: | 102.9 |
| Theta JC, top: | 29.2 |
| Theta JB: | 49.9 |
| Psi JT: | 1.5 |
| Psi JB: | 49.2 |