Hello,
we are using side A VCCA (Input) for 3.3v Master Controller and Side B VCCB (Output) for Slave RTC but when we are not communicating or Controller shutdown (3.3V Off ) at that time leakage current through the VCCB is approximately 1.6mA which is quit bigger for our application because we are using super capacitor backup supply for VCCB.
but if we connected controller side to VCCB and Slave side to VCCA and Controller shutdown (3.3V Off ) we got Leakage current of 28uA which is ok for us. but is it ok to connect in this Manner ??