Part Number: TMDS181RGZEVM
Other Parts Discussed in Thread: TMDS181, SN65DP159, TDP158, SN75DP159
Dear Support team,
Currently, an EDID emulator is connected to output HDMI 2.0 (6Gbps) from our board.
However, if an EDID emulator is connected via the TMDS181 evaluation board, 6Gbps output is not possible and the default output rate is set.
Is it necessary to modify the evaluation board when connecting the EDID enumerator via the evaluation board to perform DDC communication?
We could find below discription in the User ’s manual.
P.7
• Pop R16, R17, R24, R25. No pop R123, R124, R125, R126 - TMDS181, DDC on
• No pop R16, R17, R24, R25. Pop R123, R124, R125, R126 - TMDS181, DDC snoop only
P.18
Pop 2K resistors on R45, R46 for TMDS181, DDC on
Pop 47K resistors on R45, R46 for TMDS181, DDC snoop only
Since only DDC snoop is used in the initial state of the evaluation board, if we want to use DDC communication with the EDID emulator, should we modify EVM to DDC on condition?
Best Regards,
Hirokazu Takahashi