This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Any simpler solution for power-only (sink) PD negotiation?

Expert 6500 points

Part Number: TPS65987D

Hi, 

we would like to power our end device from USB-C port, where a USB-C charger with PD capability would deliver the power.

Basically we'd like our device to negotiate the max voltage that the charger is capable of (for instance 20V or 15V) and for this we are looking for a simple IC - the IC should negotiate that by itself, without additional control by our device (system). 

Do we have anything simpler than TPS65987D for this?

Thank you.