Part Number: DP83867IR
Hi Sir
We still can’t wake up by Magic packet.
The configuration is below:
a. Set INT_OE ->1, bit7 of CFG3(0x001E);
b. Set WOL_INT_EN ->1, bit3 of MICR(0x0012
c. RXFCFG(0x0134) -> 0x0981, level mode
d. Set MAC address, RXFPMD1~3(0x0136~0x0138),
1. MAC is 02:XX:YY:ZZ:MM:NN
2. 0x0136 -> 0xXX02
3. 0x0137 -> 0xZZYY
4. 0x0138 -> 0xNNMM
After sending magic packet(we use the tool “magic packet utility”), the INT will not pull low. Check the RXFSTS(0x0135), the read value is 0x001c.
But if we enable WAKE_ON_BCAST, after send packet, the INT will pull low.
Can you help to suggest what we need check next?