Part Number: TPS65987EVM
Other Parts Discussed in Thread: TPS65987
Hi
I am having an issue with my TPS65987EVM with 10G-EXPANSION-EVM sink board. I have previously had this setup working so I'm not sure what has changed but now when I try and output DP video from my laptop, nothing happens.
I think it is related to the HPD but am a little confused. On the hardware everything seems fine. The HPD LED is on and the monitor is switched on. However when I look at the debug registers, it shows the DP HPD is low and the PD log seems to exit alt-mode after transmitting that the HPD is low.
I have check continuity between the LED transistor gate and the HPD pin on the TPS65987 in case the Samtec connector had been damaged, but that is fine. Would this be a setting issue or is it a hardware issue?
Thanks