Part Number: TPS65982
Hi, Team
When I used TPS65982 as a Source, and I configure the PDO as 5V 3A peak current 100%, and the Sink requested 5V 900mA, then the Source OCP trip is about 1.2A;
When configure the PDO as 5V 3A peak current 200%, and the Sink requested 5V 900mA, then the Source OCP trip is about 2.2A.
So, is the Source OCP trip is the (Sink requested current * Peak current), do we have any document describe about this?
Best regards,
Picher