Part Number: LMH0341
Hello,
I have a question about the maximum current rating for the LMH0341. In the datasheet it specifies a maximum of 77 mA for the 2.5V supply in 3G with loop-through off, and a max of 120 mA on the 3.3V supply when loop-through is turned off.
Are these values absolutely never to be exceeded? Or is there some leeway with the current when designing the power circuit?