Part Number: DS90UB948-Q1
Hi
Can you please check if DS90UB948 can support 1920*1200 resolution ? because datasheet mention that 948 can support only 2048*1080
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
Hi
Can you please check if DS90UB948 can support 1920*1200 resolution ? because datasheet mention that 948 can support only 2048*1080
Yes,, it can support 1920x1200@60fps.
Please note the key spec. on how UB948 support the video resolution is PCLK freq. For ub948, it can support up to 192MHz PCLK, and can be used for 1920x1200 or 2048x1080.
best regards,
Steven
Hi steven
If Host radio send 1280*800 resolution to Deserializer (DS90UB948) , can Deserializer (DS90UB948) convert 1280*800 to 1920x1200 image ?can you share how to achieve this function ?
sorry, ub948 is one serdes for cable medium transmission, and has no video format converter mentioned by you above.
best regards,
Steven