Part Number: DS90UB953A-Q1
Other Parts Discussed in Thread: CDCI6214, DS90UB953-Q1
Hi,
in our application, we are using a 953 together with a 954.
The 953 is configured in Synchronous mode, therefore it recovers the clock from the deserializer (954).
The 954 has a PLL (CDCI6214) as clock source. This clock source provides a 25MHz clock reference.
On the serializer side, we would like to have a 50MHz clock to source an FPGA.
As the FPGA has a relative high requirement of maximum clock jitter, I would need to know if you have measured the jitter in the whole temperature range of the device, with similar configuration to the one mentioned above.
Any further information on CLK_OUT functionality is welcome.
Thanks in advanced.
Santiago