Part Number: DS250DF230
Hello expert,
Customer want to know if they can swap positive / negative signal for TX and RX in order for ease on layout. Could you kindly help to answer it? Thanks a lot!!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS250DF230
Hello expert,
Customer want to know if they can swap positive / negative signal for TX and RX in order for ease on layout. Could you kindly help to answer it? Thanks a lot!!
Best regards,
Ann Lien
Hi,
The TI retimer CDR is polarity agnostic, so CDR will be able to achieve lock and output will be present if the data and databar signals are swapped. If the user does this the output bit polarity is obviously flipped relative to input signal.
Regards,
Rodrigo Natal
HSSC Applications Engineer
Sorry, I may have misunderstood your question. It is possible for the customer to use the retimer to invert the data polarity. If the polarity for all of the FIR taps is inverted then the output polarity is flipped relative to the input. See below info taken from the programming guide.
Table. Invert the Polarity of the Output Data
|
STEP |
SHARED/ CHANNEL REGISTER SET |
OPERATION |
REGISTER ADDRESS [HEX] |
REGISTER VALUE [HEX] |
WRITE MASK [HEX] |
COMMENT |
|
1 |
Channel |
Write |
3D |
80 |
80 |
Enable FIR |
|
2 |
Channel |
Read |
3D |
Read main-cursor polarity (bit 6) |
||
|
3 |
Channel |
Read |
3E |
Read pre-cursor polarity (bit 6) |
||
|
4 |
Channel |
Read |
3F |
Read post-cursor polarity (bit 6) |
||
|
5 |
Channel |
Write |
3D |
Invert bit 6 from step 1 |
40 |
Invert the polarity bit for the main-cursor |
|
6 |
Channel |
Write |
3E |
Invert bit 6 from step 2 |
40 |
Invert the polarity bit for the pre-cursor |
|
7 |
Channel |
Write |
3F |
Invert bit 6 from step 3 |
40 |
Invert the polarity bit for the post-cursor |
Hello Rodrigo,
Thanks for your reply and will let customer know if, thanks!
Best regards,
Ann Lien
Hello Rodrigo,
Customer use two retimers on this case and they would like to know if they can change only one chip polarity and remain one chip polarity as default. Reason is that their connector is custom and the connection would be easier if they change polarity with the one chip in these two retimers. Thanks a lot!
Best regards,
Ann Lien
It would be ok to invert polarity on only one retimer and not the other.
Cordially,
Rodrigo Natal
Hello Rodrigo,
Thanks for confirmation and will let customer know it :)
Best regards,
Ann Lien