Part Number: TCAN1051HGV
Hi
We are using the TCAN1051HGV in product and want to add an external TVS on the CAN-L/H data lines as suggested as an optional additional protection in the datasheet.
The datasheet lists the following absolute maximum ratings (H-variant):
- CAN-H / CAN-L voltage range: ±70 V
- Max differential voltage between CAN-H and CAN-L: ±70 V
We want to select a TVS which ensures that the maximum limits are not exceeded and at the same time not be too restrictive.
The STMicroelectronics/ESDCAN05-2BWY has the following specs (is seems that TI does not produce a similar product?):
- Bidirectional
- VRM: 36V
- VBR(max): 43.3V
- VCL: 61V
- IPP: 3A
As the clamp is fully active at 61V (below the max limit of 70V), this seems to provide a sufficient level of protection.
We would appreciate if you could confirm/disconfirm if this is a suitable selection.
Thanks
br
Christian