Part Number: TUSB1002A
Hi Team,
I want to know what's the minimum trace length required from the host before the TUSB1002A to avoid reflection? Does 3 inch seem too short?
Thanks.
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Roy
The unmatched impedance of transmission lines causes reflections as the impedance along the length of the transmission line changes. The length of the trace is more associated with the insertion loss.
There are multiple factors that can contribute to the unmatched impedance of transmission lines. Some examples are:
Wrong calculation of transmission line impedance
Transmission line not having a solid ground reference plane
Transmission line crosses split planes
Transmission line goes through via.
Thanks
David
Hi David,
Thanks for the comments!
But let's assume the impedance is well matched but the trace length is very short, would't that cause reflection as well?
If we can make the impedance as matched as possible, do you think 3 inches is OK? Or do you need more information to determine?
Thanks.
Roy Hsu
Roy
If the impedance is well matched, then 3in trace is OK. Is there a particular issue with the 3in trace?
Thanks
David