Other Parts Discussed in Thread: AM26LV31E
We have been experiencing a number of device failures on DS26LV31 Drivers, and some DS26LV32 Receivers. When the drivers fail we notice a shorting condition to ground (or less than 5 Ohms) on one of the drivers output pairs. The circuit runs a 1 M-bit serial link between 2 different assemblies a few meters apart. The boxes are powered from 2 different DC power supplies with a common ground reference between the boxes.
The link does not have any other external protection devices (clamping diodes, Transorbs, etc). Is there a recommended configuration for external protection (I saw some recommendations on previous posts to the forum on this device)?
Are there common failure modes, or other susceptibilities to the devices (ESD, Transients, etc) especially when it appears the driver outputs are damaged?
I noticed there are also AM26LV31E series devices which have a higher ESD rating than the DS series devices. Does TI maintain any failure rates for the AM vs the DS series parts?
A schematic of the circuit can be provided.