Part Number: TFP410
Hi Expert,
Is TFP410 the right device to transfer signal from RGB signal to HDMI?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TFP410
Hi Expert,
Is TFP410 the right device to transfer signal from RGB signal to HDMI?
Hi Lenna,
Yes, but please note that the HDMI stream cannot include audio, and that the TFP410 supports pixel rates only up to 165 MHz. The maximum resolutions supported are 1080p and 1920x1200 @60Hz.
Regards,
I.K.