Part Number: TPD1E04U04
Other Parts Discussed in Thread: HD3SS3212, , ESD321
Hello, I need to add IEC 61000-4-2 Level 4 ESD protection to a USB 3.0 interface and considered the TPD1E04U04. The clamping voltage is ~9V at 16A TLP. However, the absolute maximum rating for the protected device (HD3SS3212) is Vcc + 0.5 (Vcc = 3.3V). It doesn't seem reasonable to find a voltage clamp that low. Do I misunderstand the design requirements?