Part Number: DS90UB953-Q1EVM
Hello,
My customer is trying to evaluate the EVM without a duaghter card or EVM connected (mostly evaluating power right now.) Which script should they load?
Thanks,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953-Q1EVM
Hello,
My customer is trying to evaluate the EVM without a duaghter card or EVM connected (mostly evaluating power right now.) Which script should they load?
Thanks,
Michael
Hello Michael,
What are they trying to evaluate? PATGEN from the serializer?
Best Regards,
Casey
Hi Michael,
You can use the Patgen script in the DS90UB53-Q1 datasheet in section 7.6.4. This would send a RGB8881920x1080p30 Fixed8 Colorbar pattern out from the Serializer.
Regards,
Mandeep Singh