Part Number: DS90UB960-Q1
Team,
I am targeting the DS90UB953 serializer with the DS90UB960 deserializer. I have the estimated data rate at 2Gbs with my 2 channel CSI-2. Now I am trying to find some information on the eye height that is required to have an open eye on the receiver end. It sounds like at that rate an eye height of 115mV (Section 6.6)?
Other questions:
For a two lane CSI-2 camera what should be the output?
Does the IBIS model only go up to 250MHz or 500MHz?
Thank you.