Hi guys,
I have a couple queries about this device I am hoping you can help with.
- I found this thread on choosing power rail ferrite beads:
e2e.ti.com/.../832770
My confusion is that the data sheet lists max IDD11 at 469mA and max IDD18 at 75mA, significantly less than those mentioned in the above thread. Given it is a checkerboard pattern test I doubled those currents when selecting ferrite beads.
I had initially chosen these:
VDD18: BLM18HE152SN1D which is 1.5kohm 500mA
VDD11: BLM18PG121SH1D which is 120ohm 2A. There are 3 in total. One for VDDL11, one for VDDO(A/P)11, and one for VDD(A/HS/DP/DS)11
Can you please confirm the correct current ratings? I am assume the datasheet is more reliable. - ISO 26262 - functional safety standard for the automotive industry
Are you able to confirm whether this device meets this standard or whether you will be obtaining certification for it?
Thanks, Peter