Part Number: MAX3232
Other Parts Discussed in Thread: TRS3232E,
Hi Sir
May we know what different between MAX3232CPWR/MAX3232IPWR/TRS3232EIPWR/TRS3232ECPWR parts?
if want to replace MAX3232ECUE+, which part will have benefit to suggestion?
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Chen,
The TRS3232E devices are functionally the same as the MAX3232 with added IEC61000-4-2 ESD protection which is more similar to MAX3232ECUE+.
Here is a comparison of some of the device specs.
|
Device |
Op Temp range (°C) |
ESD Protection |
|
MAX3232ECUE+ |
0 to 70 |
±15 kV (HBM) ±9 kV (IEC 1000-4-2, Contact Discharge) ±15 kV (IEC 1000-4-2, Air-Gap Discharge) |
|
MAX3232CPWR |
0 to 70 |
±15 kV HBM
|
|
MAX3232IPWR |
-40 to 85 |
±15 kV HBM
|
|
TRS3232EPWR |
0 to 70 |
±15 kV (HBM) ±8 kV (IEC61000-4-2, Contact Discharge) ±15 kV (IEC61000-4-2, Air-Gap Discharge) |
|
TRS3232EIPWR |
-40 to 85 |
±15 kV (HBM) ±8 kV (IEC61000-4-2, Contact Discharge) ±15 kV (IEC61000-4-2, Air-Gap Discharge) |
I would recommend TRS3232EPWR as a direct replacement for MAX3232ECUE+.
Let me know if you have any more questions.
Regards,
Eric