Other Parts Discussed in Thread: SN65HVD1780
Hello team,
I am using sn65hvd1780-q1.
If I use loading circuit with 4.7 Kohm as pull up/down and 47 Ohm series resistors for both outputs A and B, then how to calculate power dissipation of 47Ohm resistors during output short circut to battery voltage 16V.
Driver short-circuit output current is 200 mA.
My VCC voltage is 5V.