Other Parts Discussed in Thread: TFP401, TFP403, SN75LVDS83B, SN74CBT34X245
I'm looking at making a board which will have a single LVDS output using the SN75LVDS83B. The input to the SN75LVDS83B can either come from a TFP401 (or TFP403, I haven't decided) OR from the 24-bit output from an OMAP processor.
I would allow only 1 input set to be active at 1 time but should I buffer the inputs before the SN75LVDS83B, and if so what would be a good part?
The block diagram looks something like this:
DVI -----> TFP401 -->
|
---------> SN75LVDS83B -------> LVDS Connector
|
OMAP RGB888 --->
Thanks,
George