Part Number: USB-2-MDIO
Other Parts Discussed in Thread: MSP-EXP430G2ET
Good Morning,
I'm using the USB-2-MDIO tools on a windows 10 machine and the response time is incredibly slow. It takes ~20 seconds for each access to take place. I have the MDIO and MDC signals on an oscilloscope and I see that the transaction happens instantly, and correctly (and only once as expected). But it takes a very long time for the result to populate back to the GUI.
It's even worse when I run a script with several (~10) accesses. It takes almost 5 minutes to get the data back. Every 20 or 30 seconds I see the green and red LEDs flash once as if it's doing another access.
I'm using the latest SW, drivers, etc with a MSP-EXP430G2ET launch pad
I'm talking to a Marvell Switch, but I'm not sure if that has anything to do with it, like I mentioned before the accesses happen instantly and correctly.
Thanks