Other Parts Discussed in Thread: HD3SS215
e2e,
I am working with TMDS442 as a 1 to 2 HDMI splitter. The datasheet of the device says is supports HDMI 1.3a and my previous design I had a processor supporting resolution of 1920x1080 @ 60Hz. Do you know if it will also support HDMI 1.4b for an application with 3840x2160@30Hz. I tested the device and it seemed to work just fine. Do you have any suggestions for alternatives? It looks like this is the only 4:2 HDMI switch but possibly 2 HD3SS215s can get the job done for them.
Thank you,
Adam