Part Number: HD3SS3220
Hi all,
I'm designing an FPGA board which implements USB type-C connection.
I've chosen to use HD3SS3220 MUX/controller (configured as UFP) since my USB (device) controller supports only USB 3.0.
I've no other devices in between, so: FPGA <-> USB device controller <-> HD3SS3220 <-> USB type-C connector <-> PC/host
With reference to SLLU241A schematics on page 7, my question is: do I only need to put AC coupling capacitors (100nF) on SSTX+/- lines on the host side (pin 21,20 and 17,16), without pulldown on device side (pin 6,7)?
Moreover, do I need coupling capacitors and pull-downs on SSRX+/- lines on device side (pin 9,10)? Or they're only needed if bias from my USB device controller is above 2V?
I've already read most of the previous forum posts and the reference designs on the topic, but I would like to have a confirmation.
Thank you in advance for the replies