This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti expert :
We used the serializer is DS90UB941AS-Q1 and the deserializer is DS90UB948-Q1. The connection diagram appears as follows:
Now in our processor can visit DS90UB948 I2C addr, but DS90UB948 LVDS output single is continuous high level,for example D0- is 1.5V D0+ is 1.0V.
When I use ALP to connect DS90UB948, and set Test Pattern Mode, DS90UB948 LVDS output single is still continuous high leve.Please help me .
Thanks!
Hello,
Can you give me more details as to what you are trying to achieve? Are you trying to reduce the swing level? Are you not seeing data toggle high to low/ low to high?
Hello,
1.what you are trying to achieve?
As the question i feedback before, I wan't use DS90UB948 to output LVDS single to light up 1920x720 resolution LVDS screen. The main circuit diagram as follows:
2.trying to reduce the swing level?
Do you mean reduce the swing level of oscilloscope ?
3. data toggle high to low/ low to high?
I can't seeing data toggle high to low/ low to high in all of DS90UB948's LVDS single pins.
Hello ,
In addtion , The debugging method I have done as follows:
1.DS90UB941 link with DS90UB948 ,and DS90UB948 LOCK pin is high. Then i use usb2any to connect DS90UB948 i2c,and set DS90UB948 Test Pattern Mode in ALP. In ALP pattren generator control select enable generator and color bars, video control timing source select external.
2. Disconnect DS90UB941 use DS90UB948 alone.Use usb2any to connect DS90UB948 i2c,and set DS90UB948 Test Pattern Mode in ALP. In ALP pattren generator control select enable generator and color bars, video control timing source select internal.
Hello,
Test 1 or 2 have no display output to the screen, and DS90UB948 lvds output single is continuous high level.
we also measure DS90UB948 lvds outpu single without display screen, but the DS90UB948 lvds output single is continuous high level.