Part Number: SN65DSI84
Hi
The steady-state differential output voltage for A_Y x P/N and B_Y x P/N is 180(min) / 245(typ) / 313(max) mV when CSR 0x19 3:2 & 1:0 = 00, 100ohm near end termination.
And, It's 272mV on the real waveform below. It's matched.
However, The model 1 & 2 of LVDS output are 1.2V and 100 ohm terminal resistor.
The VOD is around = +/-500mV. Is there anything wrong in the modle of ibis file?
BR,
Wilbur.