Part Number: SN65HVD1050-EP
Other Parts Discussed in Thread: SN65HVD1050
Hi Team,
In the datasheet, it is stated that that the SN65HVD1050-EP withstands voltage transients from –200 V to 200 V, according to ISO 7637.
Could you please provide a detailed information about the duration of the transients that will not damage the device together with the other restrictions, if exist, for example source impedance for the transient or input current limitation, etc. ?
This information is important for protection circuit design.
Thanks and Regards,
Mihir