Part Number: TMDS171
Hi
I want to use it as a DVI to HDMI Retimer.
TMDS171 (OUT_D [0:2] p/n) and FPGA (HDMI Receiver) are connected.
However, with the specifications on the FPGA side, the AC coupling capacitor is required between TMDS171 to FPGA.
In this case, does the OUT_D [0:2] p/n required external termination?
best regards