This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Link status during shorted RIN pins

Part Number: DS90UB954-Q1

Hi team,

Please tell me the Link status when RIN pin is shorted.

We use 953 and 954 with differential signals.

If either RIN + or RIN- is shorted at this time, what is the link status?

1. Rin+ (or -) is shorted to GND

2. Rin+ (or -) is shorted to VDD

In this case, it looks like a single-ended input, but will FPD-LINK lost link?

Or will the link continue depending on the conditions?

3. Rin + is shorted to Rin-

In this case, there is no signal, so the link is always lost.

Is this correct?

Is this the same with the 953 DOUT?

Best regards,

Tomoaki Yoshida