This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Signal transmission problem

Hi TI team,

When serializer and deserializer transmit data through coaxial cable or STP, there will be forward and reverse data. My question is, are these two kinds of data transmitted in interval? Or superimposed together? For example, the deserializer sends an instruction to the serializer, and the serializer sends a string of data to the deserializer. This instruction and data are overlapped from the perspective of time axis? Or non overlapping? Now with the oscilloscope, it feels overlapping, but I can't understand how two digital signals, one high speed, one low speed, are superposed together, and how they are separated. Or is the oscilloscope too low?

Best Regards,
Amy Luo