Part Number: TL16C2550
Hi, staff
There are two types of TL16C2550:
TL16C2550 with operating free-air temperature of 0 to 70℃ C and TL16C2550I with -40 to +85℃.
Question
The condition of “RECOMMENDED OPERATING CONDITIONS” in the data sheet (SLWS161E) is written as “over operating free-aie temperature range”.
Is it safe to assume that the parameters (specifications) are the same for two devices with different temperature versions of TL16C2550 and TL16C2550I?
For example, is the TIMING REQUIRMENTS value of page13 considered to be a common value that can be applied to TL16C2550 and TL16C2550I?
best regards
cafain