Part Number: SN65HVD1050
Dear Sir,
I want that SN65HVD1050 Loading quantity?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The SN65HVD1050 output driver can meet ISO 11898-2 CAN physical layer requirements for differential output amplitude with effective load resistance as low as 60 Ohms. Operation down to 45 Ohms is possible with reduced output amplitude. The total effective resistive loading would be determined by the termination resistance values and the input impedance of all transceivers connected to the bus (all of these will act in parallel).
Regards,
Max