Part Number: DP83867IR
Hi, team.
could you see below and give us answer?
Q1. which point and what should customer do to check something to identify what problem is.
Q2.how to get the value of 0x0071 register
current situation,
It seems that DUT and PC are "link up" but not packet communication.
Customer couldn't resolve it, any feedback for them to do something , please tell us.
the confirmed thing they did was below.
1.power supply : no problem
2.RBIAS resister value check : 11kohm.(no problem)
3.line driver : customer designed it by following reference
4.reset signal, clock : no problem
5.register they confirmed is,,,
<Address> <value>
0x0000 0x1000
0x0001 0x796d
0x0004 0x0de1
0x0005 0xcde1
0x000A 0x0800
0x0010 0x5048
0x0011 0x6c02
6.customer tried to do self check and loop back test
customer can't get the answer from 0x0071.