Part Number: TCA9548A
Hello Together,
i am a evening student and have a Problem with a electronic circuit. We use the TCA9548A and communicate with a 5V I2C from the master device.
The Problem is following:
In the first Moment the circuit works, but after a short time the TCA9548A is not more working. the device ist "i think" broken. In the attachment I will deposit the wiring diagram and layout for you.
I do not remember where a mistake can be. I hope you can help me to solve the problem.
These is the Board Layout:
Theses is the circuit diagram: