Part Number: SN65DPHY440SS
Hello,
As introduced in the title, I wish to use the SN65DPHY440SS retimer at its max data rate (1.5 Gbps/lane) for the transmission of a MIPI CSI-2 signal over two lanes (+clock).We want to use a camera as a MIPI emitter and a Jetson Xavier dev board as a MIPI receiver.
For our design, the retimer will be located approx 20 cm away from the emitter but really close to the receiver (5 cm max).
For these requirements, I wonder after having read the datasheet what would be the advised settings to use in the retimer, especially concerning the ERC, PRE_CFG1 and VSADJ_CFG0 pins?
Thank you for your answer,
AG