Part Number: TPS65983B
Other Parts Discussed in Thread: TPS65988, TPS65987D
Is there a way to set the TPS65983 to open the power FET if the input cannot supply a certain adjustable power level (current or voltage setting)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Matt,
The first qualifier is "Only use TPS65983B if and only if the target design is implementing an Intel Thunderbolt Reference design"
My general recommendation is to consider TPS65987D or TPS65988 for a new design that needs to source 12V / 3A.
Both devices support Under Voltage Protection and will respond when VBus meets certain parameters based on Application Configuration settings and current PD contract.
Regards,
Scott