Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8020B-Q1: hardware disign

Part Number: TUSB8020B-Q1

Hi,

A TUSB8020B-Q1 is used in my mainboard, and the mainboard doesn't supply VBUS for external USB device. In this case ,how to use pin OVERCUR1z ,pin PWRCTL_POL/SS_DN1 and pin GANGED/SMBA2/HS_UP?

Thank you.

Best Regards.

Gavin.

  • Hi Gavin,

    OVERCURXz  pins should be connected to the VBUS power switch fault pin or can be pulled high to 3.3V . If the polarity of the PWRCTL is okay as active high, PWRCTL_POL can be left floating. If downstream port power should be controlled separately then GANGED needs a pull up resistor otherwise can be left unconnected. If the main board has no control over DFP Vbus then FULLPWRMGMT should be pulled up. 

    Note: Overcurrent reporting required for USB-IF Compliance.