Part Number: TLK110
Dear all,
The same phenomenon as the following E2E link is occurring in our customers.
Along with that, I have been asked by them the conditions to link up when TLK110 is OFF.
If TLK110 is OFF and your link partner is under the following conditions, please let me know if you want to link up.
・When the communicating partner device (link partner) is used at a forced 10Mbps
・When the communicating partner device (link partner) is used at a forced 100Mbps
・ When is judged as 10Mbps by ANEG (auto negotiation)
・ When it is judged as 100Mbps by ANEG (auto negotiation)
I hope you can get a reply as soon as possible.
Best Regards,
Y.Ottey