Part Number: DP83822IF
Other Parts Discussed in Thread: DP83822I
Hi
DP83822IF VOD is 1.75V(typ) at 10BASE-Te.
If customer want to receive with 10BASE-T(2.5V,typ). Can the DP83822IF support this configuration?
Muk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Muk,
Please refer to Table 74 in the DP83822 datasheet.
Thanks,
Vibhu
Vibhu-san,
I know, DP83822 can select Line Driver Swing. However, there is not setting for 10Base-T(Typ2.5V) .
Also, I found the following sessions regarding output swing. My understanding is DP83822 is for 10BASE-Te. DP83822 cannot select the voltage swing for 10BASE-T. Is it correct?
If you have recommended method, please let me know.


Hello Muk-san,
Sorry for the misinterpretation. You are correct the DP83822 is for 10BASE-Te.
Thanks,
Vibhu
Dear Vibhu-san
I'm Suzuki.
I want to ask a basic question.
Can DP83822I connect to the device that supports only "10BASE-T"?
Regards,
T.Suzuki
Hello Masa-san,
DP83822 only meets the standard for 10BASE-Te and not 10BASE-T. Correct.
"In 10BASE-Te operation, EEE operates with a reduced transmit amplitude that is fully interoperable with a 10BASE-T PHY."
The above statement means that the DP83822 can link and operate with a link partner that is 10BASE-T. The 10BASE-T link partner generally will have a receiver that accepts the voltage swing of 10BASE-Te.
Thanks,
Vibhu
Hi, Vibhu-san
I've been asked by Customer to know below comment is from IEEE standard or out thought.
Does IEEE standard define below ?
The above statement means that the DP83822 can link and operate with a link partner that is 10BASE-T. The 10BASE-T link partner generally will have a receiver that accepts the voltage swing of 10BASE-Te.
Hello Masa-san,
Please take a look at this http://www.ieee802.org/3/az/public/apr09/grimwood_01_0409.pdf
Thanks,
Vibhu