Part Number: XIO2213B
Hi Sir,
If I have two XIO2213B cards on the same PC,
How do I distinguish between A Card or B Card? pass through Address? Or how to set the internal register?
Hugo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello-
Let me research a bit and I will get back to you in a day or two.
Regards,
Davor
Hello-
Typically the serial EEPROM is programmed to have a Global Unique ID (GUID). Each XIO2213B loads the EEPROM data at power-up including the GUID (See datasheet Section 3.5.3) . The GUID is used to distinguish between the two cards.
Regards,
Davor